Add a plug-in module to the controller
Use plug-ins to expand
Micro800
controllers for extra I/Os, communications, memory backup, and specialty capabilities.To add a plug-in module to the controller
- InProject Organizer, go to .
- Right-clickPlug-in, and then selectNew module.
- InAdd module, select a plug-in module, and then selectAdd.
- InDevices definition, configure the slot, revision, and controller fault settings, and then selectOK.TIP: To open the configuration page of a plug-in module, inProject Organizer, double-click<plug-in-ID>.
Provide Feedback