Independently released expansion modules
Each release of
FactoryTalk Design Workbench
includes a set of expansion modules for the L50E and L70E controllers. You can add the expansion modules to the controllers and configure the expansion modules using the controller workspace.Some expansion modules are released and available independently from the software release, and come with a support package that, when installed, updates the
FactoryTalk Design Workbench
software.After you add an independently released expansion module, the expansion module is available in
Project Organizer
under the Expansion
node. Configuration and management of independently released expansion modules follow the same procedure as other expansion modules.Provide Feedback