Delete an expansion module from the controller
Deleting an expansion module removes all associated variables from the controller configuration.
After deletion, update the Project Organization Units, interrupt definitions, Modbus address mappings, MicroLogix mappings, and DNP3 mappings that use these variables.
To delete an expansion module from the controller
- InProject Organizer, go to .
- ExpandExpansion, right-click the expansion module, and then selectDelete.
- InWarning:
- SelectOKto remove the placeholder fromProject Organizer. The slot numbers of subsequent modules will reduce by one.
- SelectNoto keep the placeholder inProject Organizer, withAvailableappearing at the original slot. The slot numbers of other modules remain unchanged.
Provide Feedback