Run Data Transformation

Perform the following steps to run data transformation:
  1. In the Mapping editor, click
    Run
    and select
    Run with client credentials
    .
    You should now see the label
    configured
    , when you select
    Run with client credentials
    .
    Select Run with Client Credentials
  2. Click
    Run with client credentials
    .
  3. You can view the transformation data under Run History.
    View Transformation Data
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal