Configuring Grafana to connect to FactoryTalk DataMosaix

Perform the following steps to configure Grafana to connect to FactoryTalk DataMosaix:
  1. Register the application in FactoryTalk DataMosaix. For information on registering an application in FactoryTalk DataMosaix, refer to Register Application.
  2. Download and Install Grafana (available on Chocolaty GUI). Check if the service is running.
  3. Navigate to localhost:3000 (Default port).
  4. Provide Username:admin and password:admin. It is recommended you to update the password.
  5. Install the Cognite Data Fusion plugin.
    • Navigate to menu >
      Administrations
      >
      Plugins
      .
    • Search and navigate to
      Cognite Data Fusion
      and click
      Install
      .
  6. Create a new data source in the Cogite Data Fusion portal.
    • Navigate to menu >
      Connections
      >
      Connect data
      .
    • Search and navigate to
      Cognite Data Fusion
      .
    • Create a new data source by clicking
      Create a Cognite Data Fusion DataSource
      .
    • The data source is created.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal