Prerequisites
- Tableau Cloud/Desktop is installed. For more information, refer to Download Tableau.
- License for Tableau Cloud/Desktop.
- Postgres JDBC driver is installed, refer to Driver Installation.NOTE:The driver should be installed on the machine that will run the Tableau Desktop client to connect Tableau with the PostgreSQL server.
- Access to FactoryTalk DataMosaix.
- Register the application using the Machine-to-Machine type in FactoryTalk DataMosaix. For information on registering an application in FactoryTalk DataMosaix, refer to Register Application.
Provide Feedback