Requirements
Minimum Software and Hardware Requirements
Operating System | Hardware |
|---|---|
Windows 10 orWindows 11 orWindows Server 2019 orWindows Server 2022 | Storage : 80 MB of available hard disk space.RAM : 512 MB. |
Prerequisites
- Microsoft.NET Framework 4.6 is installed.
- Access toFactoryTalk DataMosaix SaaSis available.
- The user has the Data Scientist role assigned within theFactoryTalk DataMosaix SaaSapplication. This role is required to create applications.
- The application is registered inFactoryTalk DataMosaix SaaSusing the Machine-to-Machine application type. For more information on registering an application inFactoryTalk DataMosaix SaaS, refer to Register Application.
Provide Feedback