Configure SSRS to connect to a Virtual PostgreSQL Data Interface
Perform the following steps to configure SSRS to connect to a virtual PostgreSQL data interface:
- Click here to navigate to theMicrosoftReport Builder download page.Alternatively, you can paste the following URL in your browser's address bar and pressEnter.https://www.microsoft.com/en-us/download/details.aspx?id=53613
- ClickDownload.Click Download
TheReportBuilder.msifile will be downloaded in the Downloads folder of your local machine. - Double-click theReportBuilder.msifile.TheMicrosoft Report Builderdialog box is displayed.
- ClickNext.Microsoft Report Builder Dialog

- Select theI accept the terms in the license agreementoption.
- ClickNext.License Agreement

- In theFeature Selection, clickNext.Feature Selection

- In theDefault Target Server, clickNext.NOTE:If the target server URL differs from the default, provide the new URL in theDefault target server URL (Optional)box.Default Target Server

- ClickInstall.Click Install

- Once the installation is completed, clickFinish.Click Finish

- Click here to navigate to the ODBC driver download page.Alternatively, you can paste the following URL in your browser's address bar and pressEnter.https://www.postgresql.org/ftp/odbc/releases/REL-17_00_0004-mimalloc/
- Clickpsqlodbc-setup.exe.Click Setup File
Thepsqlodbc-setup.exefile will be downloaded in the Downloads folder of your local machine. - Double-click thepsqlodbc-setup.exefile.Thepsqlodbc Setupdialog box is displayed.
- Select theI agree to the license terms and conditionscheckbox.
- ClickInstall.Psqlodbc Setup Dialog

- Once the installation is completed, clickClose.Click Close

- Open theODBC Data Source Administratorfrom your local machine.
- In theODBC Data Source Administratordialog box, underUser DSNtab, clickAdd.NOTE:Users can also select theSystem DSNtab to create a new data source.ODBC Data Source Administrator Dialog

- In theCreate New Data Sourcedialog box, clickPostgreSQL ANSI.
- ClickFinish.Create New Data Source Dialog

- In thePostgreSQL ANSI ODBC Driver (psqlODBC) Setupdialog, perform the following actions:
- Data Source: By default, the data source name is displayed. The user can also provide the unique name for the data source.
- Description (Optional): Provide a description for the data source.
- Database: The name of the project inFactoryTalk DataMosaix SaaS. For example, Check-46
- SSL Mode: Select therequiremode from the drop-down list.
- Server:dm-virtualpostgres.cloud.rockwellautomation.com(Production URL).
- Port: Provide the port number as5432.
- Username: Refer to the Client ID generated while registering the application.
- Password: Refer to the Client Secret generated while registering the application.
- ClickTest.PostgreSQL ANSI ODBC Driver (psqlODBC) Setup Dialog

- Once the test connection is successful, theConnection Testdialog box is displayed and clickOK.Connection Test Dialog

- In thePostgreSQL ANSI ODBC Driver (psqlODBC) Setupdialog box, clickSave.Click Save
In theODBC Data Source Administratordialog box, the user can view the PostgreSQL data source name. - ClickOK.ODBC Data Source Administrator Dialog

- Open theMicrosoft Report Builderfrom your local machine.
- Right-click theDatasetsfrom the left pane and clickAdd Dataset….Click Add Dataset

- In theDataset Propertiesdialog box, select theUse a dataset embedded in my reportoption.
- ClickNew.Dataset Properties
TheData Source Propertiesdialog box is displayed. - Select theUse a connection embedded in my reportoption.
- SelectODBCfrom theSelect connection typedrop-down list.
- ClickBuild.Data Source Properties Dialog

- In theConnection Propertiesdialog box, select theUse user or system data source nameoption and select thePostgreSQL30from the drop-down list.
- ClickTest Connection.Connection Properties Dialog

- Once the test connection is successful, theTest resultsdialog box is displayed and clickOK.Test Results

- In theConnection Propertiesdialog box, clickOK.Connection Properties

- In theData Source Propertiesdialog box, clickOK.Data Source Properties

- Right-click the newly created datasets and clickQuery.Click Query

- In theQuery Designerdialog box, provide the sample query and click the [
] icon to run the query.Run Query
Based on the query, the final data will be populated.Final Output
Provide Feedback