Creating a New Deviation Label
If none of the first principle recommendations apply, a user can choose to create a new label. To do so, a user should select the “Other” radio button and click on Add New.
Other & Add New Deviation Label

A dialogue box is displayed with the fields to create the new failure Risk label. The label includes the name, descriptions, and prescription (optional).
Creating a New Failure Risk

Upon creating the new label, the user can associate severity and recommended time to resolve the deviation.
Severity and Time to Resolve

Provide Feedback