Configure SMTP Server

To configure the SMTP Server, a user should first go to the Notifications settings by selecting the gear icon in the upper right of the application. The edge node hosting FactoryTalk Analytics GuardianAI should have visibility to the network hosting the SMTP server. To establish the connection, the following parameters will need to be configured. It may be required to consult with an IT department to obtain an SMTP server:
  1. Server Domain
    : The domain address of the SMTP server (consult with IT).
  2. Port Number
    : SMTP server port, common ports may be 25, 465, or 587 (consult with IT).
  3. Email Id
    : The email ID displayed to the email recipient (example:abc.def@xyz.com).
  4. Username
    : Username to authenticate with the SMTP server (consult with IT).
  5. Password
    : Password to authenticate with the SMTP server (consult with IT).
  6. SSL Connection (optional)
    : Enable SSL encryption when communicating between FactoryTalk Analytics GuardianAI and the SMTP server.
SMTP Server Configuration
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal