Security Considerations for FactoryTalk Analytics GuardianAI
When deploying FactoryTalk Analytics GuardianAI within operations considerations should be applied to the physical and cyber system security posture of the system. The FactoryTalk Analytics GuardianAI application is designed to run as an edge application either on FactoryTalk Edge Manager or on a client supplied edge hardware and infrastructure.
System security is a paramount tenet of overall operation success. The following document and links are being provided as guidance on best practices of how to implement system security principles within industrial automation control systems. It is of best practice for users of FactoryTalk Analytics GuardianAI to follow these practices to provide the best level of defense in depth security for their overall systems
Publication Name | Description | Link |
|---|---|---|
Converged Plantwide Ethernet (CPwE) Design | Converged Plantwide Ethernet Design Implementation Guide | |
Deploying Firewalls within CPwE Architecture | Use cases for designing, deploying, and managing industrial firewalls | |
Deploy Identity and Mobility Services | Guidelines for protecting systems through deploying centrally managed defense in-depth security approach | |
Secure Cloud Connectivity to CPwE | Application guide for securing cloud applications within CPwE Architecture | Secure Cloud Connectivity to CPwE |
Deploy CIP Security within CPwE | Network security use cases for CPwE systems | |
Deploy CIP Security within CPwE | IEC 62443 security architecture use cases and design principles | |
Physical Infrastructure within CPwE Architecture | Use cases for deploying robust physical infrastructure for industrial applications | |
Provide Feedback