Device definition dialog box - Commands view parameters

Parameter
Description
Available
Displays the names of all supported Commands. The list does not include commands contained in the
Selected
command list. Right click to sort the list.
  • Sort by number
  • Sort by name
  • Sort by type
Use the
Add
and
Remove
button to move device variables between the lists.
Selected
Displays the list of commands selected for use. The
Selected
list can contain four Commands (maximum) for both PlantPAx and non PlantPAx.
Use the
Add
and
Remove
button to move device variables between the lists.
Command details
Displays the name, HART data type, initial value and parameter type for each selected command.
The available values for the
Parameter Type
column are
Request
and
Response
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal