Add/Edit VLAN dialog box parameters
The
Add/Edit VLAN
dialog box includes these parameters:Parameter | Description |
---|---|
VLAN ID | Specifies the ID name. The ID must be numeric, unique, and within the range from 2 through 1001 or 1006 through 4094. |
VLAN Name | Specifies the VLAN name. The VLAN names must be unique and not more than 20 characters in length. |
Set | Sends the settings to the switch and closes the dialog box. The Enter Password dialog box may appear. |
Provide Feedback