Parallel Redundancy Protocol view parameters
The
Parallel Redundancy Protocol
view includes the following parameters:Parameter | Description |
---|---|
Channel Group 1 | Shows the PRP ports for Channel Group 1 . |
Port A | Shows the PRP port for LAN A. |
Port B | Shows the PRP port for LAN B |
Channel Group 2 | Shows the PRP ports for Channel Group 2. Only available for Stratix 5410 switch. |
Refresh | Retrieves and displays the latest values from the device. |
Provide Feedback