Cable Diagnostics dialog box
Use the
Cable Diagnostics
dialog box to diagnose a cable problem:- Run Cable Diagnostic test
- View status of the cables
IMPORTANT:
- For a valid cable test for gigabit ports, you must first configure the gigabit port as a RJ45 media type in the Device Manager Web interface.
- The test can interrupt connections to the device and any device connected through the device. The test can also interrupt the connection between the workstation and the controller.You must have the correct privilege to run the test.
TIP:
The parameters in this view are available while online.
Provide Feedback