Device definition dialog box parameters
The
Device definition
dialog box includes these parameters:Parameter | Description |
---|---|
Device type | Displays the device catalog number and type. |
Name | Enter an IEC 61131 compliant device name. If an invalid character is entered in this field, or if the name exceeds 40 characters, the software ignores the character. |
Description | Enter the description of the device. Tip : The description must be within 128 characters. If the description exceeds the maximum length, the software ignores any extra characters. |
Ethernet address | Specifies the IP configuration for the device. Possible options include:
|
Revision | Choose the appropriate major and minor revision of the device. Use the major revision to indicate the revision of the interface to the device. Set the major revision. The default value for the major revision is 1. Use the minor revision to indicate the firmware revision. Set the minor revision between 1 and 255. The default value for the minor revision is 1. The major revision feature is not available in online mode. The minor revision feature is not available in Run mode. |
Electronic keying | Specifies the electronic keying to use for the selected device. Valid values are:
Electronic keying is enabled while offline, and while in these modes:
Electronic keying appears shaded in Run mode.For more information on Electronic Keying, see Electronic Keying in Logix 5000 Control Systems Application Technique, publication LOGIX-AT001.IMPORTANT :
|
Connection | Specifies the type of I/O connection to use between the device and the controller. The available values are:
Connection is not available in online mode.IMPORTANT : To disable a port set the corresponding output tag. Setting Connection to Data overwrites any previous setting performed through Device Manager, CLI, or CNA. |
Data connection password | Specifies the password to the switch. This feature is only available when you set the Connection to Data . Passwords can contain up to 63 characters and are case sensitive. Valid characters include:
Tip : The password cannot include embedded spaces. |
Provide Feedback