NTP Client view
Use the
Network Time Protocol Client
view to view NTP status and to add and delete NTP server addresses.Use the
Network Time Protocol Client
view to:- View whether the NTP is enabled and the clock is synchronized, and the current time.
- View the NTP server status.
- Add NTP server addresses.
- Specify the preferred NTP servers.
- Delete NTP server addresses.
The NTP client and NTP server status information is only shown when NTP is enabled on the switch and the switch is online.
Provide Feedback