Add NTP Server dialog box parameters

The
Add NTP Server
dialog box includes these parameters:
Parameter
Description
NTP Server Address
Specifies the IP address of the NTP server. Available values:
  • Class A (Netid.hostid.hostid.hostid): 1.0.0.0 to 126.255.255.255
  • Class B (Netid.Netid.hostid.hostid): 128.0.0.0 to 191.255.255.255
  • Class C (Netid.Netid.Netid.hostid): 192.0.0.0 to 223.255.255.255
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal