Public to Private Translations - InstanceX dialog box parameters
The
Public to Private Translations - InstanceX
dialog box includes these parameters:Parameter | Description |
---|---|
Public | Displays the unique IP address on the public subnet that represents the corresponding IP address on the private subnet. |
Private | Displays the IP address on the private subnet that was changed to a unique IP address on the public subnet. |
Subnet | Indicates whether the translation is part of a Subnet entry type. |
Number of Packets | Displays the number of packets for each translation. |
Provide Feedback