Private to Public Translations - InstanceX dialog box parameters
The
Private to Public Translations
- InstanceX
dialog box includes these parameters:Parameter | Description |
---|---|
Private | Displays the existing address for a device on the private subnet. |
Public | Displays a unique public address that represents the corresponding device on the private subnet. |
Subnet | Indicates whether the translation is part of a Subnet entry type. |
Number of Packets | Displays the number of packets for each translation. |
Provide Feedback