NAT view

Use the
NAT
view to create and modify Network Address Translation (NAT) instances. A NAT instance contains entries that define each address translation, as well as other configuration parameters.
In the
NAT
view, you can:
  • Delete a NAT instance.
  • Create a NAT instance.
  • Edit an existing NAT instance.
  • View diagnostics information about a NAT instance.
  • View diagnostics data for all NAT instances.
The data is only displayed when the device is online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal