Add/Edit NAT Instance - Public to Private view parameters
The
Public to Private
view includes these parameters:Parameter | Description |
---|---|
Public | Displays the unique public IP address. |
Private | Displays the unique private IP address. |
Subnet Mask | Displays the subnet mask. |
![]() | Deletes the table entry. |
![]() | Creates a new public IP address that will be translated to an IP addresses on the private subnet. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. |
Provide Feedback