Add/Edit NAT Instance - Overview view

Use the
Overview
view to configure a NAT instance.
In the
Overview
view, you can:
  • Create a new private IP address that will be translated to an IP address on the public subnet.
  • Assign a VLAN to a NAT instance.
  • Enable devices on the public subnet to communicate with devices on the private subnet.
Any row in the
Private to Public
table that has not been sent to the switch is denoted by an asterisk.
The parameters are active and data displayed only when the switch is online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal