Add/Edit NAT Instance - Advanced view parameters
The
Advanced
view includes these parameters.Parameter | Description |
---|---|
Traffic Permits | The types of incoming and outgoing packets that are not handled by NAT.
|
Incoming | Specifies how to handle each type of incoming packet.
|
Outgoing | Specifies how to handle each type of outgoing packet.
|
Fixup Packets | Indicates that the fixup protocols are enabled. If cleared, the fixup protocols are disabled.
|
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. The Enter password dialog box may appear. |
Provide Feedback