NAT Diagnostics - InstanceX dialog box parameters

The
NAT Diagnostics - InstanceX
dialog box contains these parameters.
Parameters
Description
Current Active Translations
Displays the number of translations that have occurred within the last 90 seconds across all NAT instances.
Total NAT Translated Packets
Displays the total number of packets that have been translated for this NAT instance.
Total Private to Public Address Translations
Displays the total number of private-to-public translations for this NAT instance.
Total Public to Private Address Translations
Displays the total number of public-to-private translations for this NAT instance.
Total Translations
Displays the total number of private-to-public and public-to-private translations for this NAT instance.
ARP Fixup Packets
Displays the number of ARP (Address Resolution Protocol) packets that have been fixed up for this NAT instance.
ICMP Fixup Packets
Displays the number of ICMP (Internet Control Message Protocol) packets that have been fixed up for this NAT instance.
Total Fixups Packets
Displays the number of ARP and ICMP packets that have been fixed up for this NAT instance.
Blocked Non-Translated Traffic Packets
Displays the number of packets with untranslated traffic that were blocked for this NAT instance.
Pass-Through Non-Translated Traffic Packets
Displays the number of packets with untranslated traffic that were passed through for this instance.
Blocked Multicast Traffic Packets
Displays the number of packets with multicast traffic that were blocked for this NAT instance.
Pass-Through Multicast Traffic Packets
Displays the number of packets with multicast traffic that were passed through for this NAT instance.
Blocked IGMP Traffic Packets
Displays the number of packets with IGMP (Internet Group Managed Protocol) traffic that were blocked for this NAT instance.
Pass-Through IGMP Traffic Packets
Displays the number of packets with IGMP traffic that were passed through for this NAT instance.
Private to Public Translations
Opens the
Private to Public Translations
dialog box to view private-to-public translation diagnostics for the instance.
Public to Private Translations
Opens the
Public to Private Translations
dialog box to view public-to-private translation diagnostics for the instance.
Refresh
Retrieves and displays the latest values from the device.
Clear Diagnostics
Clears the diagnostic totals for this NAT instance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal