DHCP Address Assignment view

Use the
DHCP Address Assignment
view to view and configure DHCP persistence. The Dynamic Host Configuration Protocol (DHCP) automatically assigns IP address information from a pool of available addresses to newly connected devices (DHCP clients) in the network. If a device leaves and then re-joins the network, the device receives the next available IP address, which might or might not be the same address that it had before.
Set the switch to operate as a DHCP server to provide DHCP persistence. With DHCP persistence, you can assign a specific IP address to each port, ensuring that the device attached to a given port gets the same IP address.
The data is only displayed when the device is online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal