Advanced dialog box parameters for the DHCP view

The
Advanced
dialog box includes these parameter:
Parameter
Description
Enable DLR DHCP Snooping
Indicates whether Dynamic Host Configuration Protocol (DHCP) snooping is enabled or disabled for the Device Level Ring (DLR).
When enabled, broadcast of DHCP requests are restricted beyond the connected switch. As a result, devices only receive address assignments from the connected switch.
This option is available on VLAN interfaces.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal