Search
1783 Stratix Switch
Manage the Switch
Add or edit an NAT instance
Add an NTP server address
Assign a precedence value to the ring supervisor
Assign an IP address to a DHCP port
Clear a fault on a ring
Configure a switch using express setup
Configure the DLR network
Configure ports for changes at controller
Configure the DHCP
Configure the NTP client
Configure the Power over Ethernet ports
Configure the redundant gateway
Copy configuration files or IOS image
Create a new DHCP pool
Create or edit a VLAN
Create or edit an EtherChannel group
Delete a DHCP pool
Delete a VLAN
Delete an NAT instance
Delete an NTP server address
Diagnose a problem with the link
Edit a DHCP pool
Enable time synchronization
Enable an uplink port
Enter a password
Export the switch configuration
Import a switch configuration
Monitor DLR status
Refresh communication with the switch
Reset a device
Reset the port diagnostic counters
Reset the ring fault counter
Reset the PRP diagnostic counters
Run Diagnose Cable test
Send configuration settings to the switch
Sort ring members
Starting Private IP Address
Starting Public IP Address
Transition to Run mode behavior
Upload/download a switch configuration file
Verify the last fault location on a port
View port diagnostics
View statistical information about the ring
View the status of the PRP network
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal