Sensor

Information - Active Type

(class 0x311, instance 1-8, attribute 2)
Configured sensor type.
Sensor Type encoding
Value
Sensor Type
0
---
1
Oxygen (amp.)
2
Oxygen (opt.)
3
pH Glass
4
E_SensorKSG2_deprecated
5
pH ISFET
6
Cond c
7
Cond i
8
ORP
9
TU/TS
10
Nitrate
11
ISE (CAS40D)
12
SAC
13
Ultrasonic interface (CUS71D)
14
Chlorine (CCS142D)
15
E_SensorFSPH1
16
E_SensorFSLC1
17
E_SensorFSLI1
18
pH/ORP
19
Cond c 4-pol
20
Oxygen (opt.)
21
TU
22
Inline photometer
23
TU/AU
24
Disinfection
25
Spectrometer
26
Oxygen (amp.)
27
E_SensorKSR2_deprecated
28
Fluorescence
29
ISE (CAS41E)
30
Ultrasonic interface
31
DPD Analyzer module

Information - Serial Number

(class 0x311, instance 1-8, attribute 5)
The serial number of the sensor.

Information - Connected Type

(class 0x311, instance 1-8, attribute 3)
Connected sensor type. The connected sensor type shall match the configured sensor type.
Connected Sensor Type encoding
Value
Connected Sensor Type
0
---
1
Oxygen (amp.)
2
Oxygen (opt.)
3
pH Glass
4
E_SensorKSG2_deprecated
5
pH ISFET
6
Cond c
7
Cond i
8
ORP
9
TU/TS
10
Nitrate
11
ISE (CAS40D)
12
SAC
13
Ultrasonic interface (CUS71D)
14
Chlorine (CCS142D)
15
E_SensorFSPH1
16
E_SensorFSLC1
17
E_SensorFSLI1
18
pH/ORP
19
Cond c 4-pol
20
Oxygen (opt.)
21
TU
22
Inline photometer
23
TU/AU
24
Disinfection
25
Spectrometer
26
Oxygen (amp.)
27
E_SensorKSR2_deprecated
28
Fluorescence
29
ISE (CAS41E)
30
Ultrasonic interface
31
DPD Analyzer module

Information - HW version

(class 0x311, instance 1-8, attribute 6)
Hardware version of the device.

Information - SW version

(class 0x311, instance 1-8, attribute 7)
Software version of the device.

Information - Enabled

(class 0x311, instance 1-8, attribute 1)
On: The channel display is switched on in the measuring mode
Off: The channel is not displayed in the measuring mode, regardless of whether a sensor is connected or not.
Channel Enable encoding
Value
Channel Enable
0
On
1
Off

Information - Tag

(class 0x311, instance 1-8, attribute 4)
"Tag" stands for the name of a measuring point, and is used in many areas of process measuring technology. If the TAG control function is activated, the controller checks every sensor to be connected as to whether this sensor belongs to the measuring point, and only accepts the sensors that have the same tag.

Operating Time - Total

(class 0x311, instance 1-8, attribute 31)
Operation time of the sensor in seconds.

Operating Time - Initial operation date

(class 0x311, instance 1-8, attribute 11)
Initial operation date of the sensor.

Operating Time - Above spec. temp.e

(class 0x311, instance 1-8, attribute 32)
Total time the sensor is operated above its maximum operation temperature.

Operating Time - Below spec. temp.

(class 0x311, instance 1-8, attribute 33)
Total time the sensor is operated below its minimum operation temperature.

Data Set Switch - SAC

(class 0x311, instance 1-8, attribute 41)
Calibration data records are saved under an individual name in the sensor. A new sensor is calibrated at the factory and thus already has appropriate data records. You can add your own data records during each calibration. These are then available for selection under "Application".
SAC Data Set encoding
Value
Data Set
0
E_DSID_Factory
1
E_DSID_NICustomer1
2
E_DSID_NICustomer2
3
E_DSID_NICustomer3
4
E_DSID_NICustomer4
5
E_DSID_NICustomer5
6
E_DSID_NICustomer6
7
E_DSID_NIUndefined

Data Set Switch - Nitrate

(class 0x311, instance 1-8, attribute 42)
Calibration data records are saved under an individual name in the sensor. A new sensor is calibrated at the factory and thus already has appropriate data records. You can add your own data records during each calibration. These are then available for selection under "Application".
Nitrate Data Set encoding
Value
Data Set
0
E_DSID_Factory
1
E_DSID_NICustomer1
2
E_DSID_NICustomer2
3
E_DSID_NICustomer3
4
E_DSID_NICustomer4
5
E_DSID_NICustomer5
6
E_DSID_NICustomer6
7
E_DSID_NIUndefined

Data Set Switch - Turbidity

(class 0x311, instance 1-8, attribute 43)
Calibration data records are saved under an individual name in the sensor. A new sensor is calibrated at the factory and thus already has appropriate data records. You can add your own data records during each calibration. These are then available for selection under "Application".
Turbidity Data Set encoding
Value
Data Set
0
E_DSID_FactoryFNU
1
E_DSID_FactoryKaolin
2
E_DSID_FactorySIO2
3
E_DSID_FactoryTIO2
4
E_DSID_FactARALeakage
5
E_DSID_FactARASludge
6
E_DSID_FactARASludgeActiv
7
E_DSID_TUCustomer1
8
E_DSID_TUCustomer2
9
E_DSID_TUCustomer3
10
E_DSID_TUCustomer4
11
E_DSID_TUCustomer5
12
E_DSID_TUUndefined
13
E_DSID_FactoryLDSludgeActive
14
E_DSID_FactoryPSL
15
E_DSID_FactoryKieselguhr
16
E_DSID_TUCustomer6
17
E_DSID_FactoryAU
18
E_DSID_DoNotUseThisSludge
19
E_DSID_EBC
20
E_DSID_Milk
21
E_DSID_Apha
22
E_DSID_EBCColor
23
E_DSID_OEM1
24
E_DSID_OEM2
25
E_DSID_OEM3
26
E_DSID_OEM4
27
E_DSID_OEM5
28
E_DSID_OEM6
29
E_DSID_Productloss
30
E_DSID_Sludge
31
E_DSID_AutoSludge
32
E_DSID_TUCustomer7
33
E_DSID_TUCustomer8
34
E_DSID_Thickener
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal