Current Outputs
Process Value - Value
(class 0x310, instance 1, attribute x)
Process Value in its Engineering Unit which is mapped to analog current output.
Channel | Attribute number |
|---|---|
1 | 110 |
2 | 113 |
3 | 116 |
4 | 119 |
5 | 122 |
6 | 125 |
7 | 128 |
8 | 131 |
Process Value - Unit
(class 0x310, instance 1, attribute x)
Engineering Unit. Encoding see EtherNet/IP manual.
Channel | Attribute number |
|---|---|
1 | 112 |
2 | 115 |
3 | 118 |
4 | 121 |
5 | 124 |
6 | 127 |
7 | 130 |
8 | 133 |
Process Value - Status
(class 0x310, instance 1, attribute x)
Status of the Process value.
Value | Status |
|---|---|
0 | Bad: NotConnected. Never transmitted from the device, EDS offline default
value. |
4 | Bad: ConfigurationError. Set if no process value is mapped to the device
variable AIx/DIx. |
12 | Bad: DeviceFailure. Set if the device cannot provide a valid value due to an
error. |
64 | Uncertain: NonSpecific. Set if the device cannot provide an accurate value due
to an error. |
128 | Good: OK. The value is valid |
Channel | Attibute number |
|---|---|
1 | 111 |
2 | 114 |
3 | 117 |
4 | 120 |
5 | 123 |
6 | 126 |
7 | 129 |
8 | 132 |
Current Value
(class 0x310, instance 1, attribute x)
Current Value in mA which is mapped to the current analog output.
Channel | Attribute number |
|---|---|
1 | 134 |
2 | 135 |
3 | 136 |
4 | 137 |
5 | 138 |
6 | 139 |
7 | 140 |
8 | 141 |
Provide Feedback