Documentation
Manual
The primary sources of detailed module information is the Liquiline CA8xxx EtherNet/IP
manual. It can be found on the CD or on the Endress+Hauser website (Liquiline CA80AM).
EDS File
The EDS file is used for identifying the module to network tools, such as RSLinx, RSNetWorx
or a CIP (refer to "CIP" in RSLogix5000 HELP) network browser (e.g. RSLinx Who). It can also
be downloaded from the Endress+Hauser website. The EDS file is installed using the RSLinx
Hardware Installation Tool. The EDS file can also be directly loaded from the device using
RSLinx.
Provide Feedback