Device Diagnostics parameters

The
Device diagnostics
dialog box is used for multiple device types so the parameters displayed can vary. Settings that do not apply to a device type do not appear.
TIP:
When the connection is lost to the device, a timeout error occurs. On dismissal of the error message, the parameters are blank.
Parameter
Description
Run mode
Shows the operating state for the device.
Output devices follow the Run Mode for the owning connection.
Input-only devices are always in Run Mode.
The available values are:
  • Idle
  • Run
Diagnostics thresholds exceeded
Shows whether any diagnostics are active or a threshold has been reached.
The available values are:
  • None
    . No diagnostics active
  • Yes
    . One or more diagnostic thresholds reached
Diagnostics sequence count
Shows the count for each time a distinct diagnostic condition was detected, and also each time a distinct diagnostic condition transitioned from detected to not detected.
Available values range from 0 to 255.
Self test
Shows whether internal product initialization tests detected an error.
The available values are:
  • Passed
  • Failed
CPU utilization
Shows the usage of the compute engine.
Available values range from 0% to 100%.
Chassis status
Shows whether the chassis is operating normally.
Redundant
Shows whether the device is running in Redundant mode.
Tip: If the device is not intended to run in Redundant mode, the value is always
No
, but if the device is intended to run in Redundant mode and the value is
No
, this indicates there is a problem.
The available values are:
  • True
  • False
Memory card status
Shows the current status of the removable memory card.
The available values are:
  • Fault
    . Removable memory card is either not present, not formatted, or has insufficient space available to store configuration data and firmware
  • OK
    . Removable memory card is present, formatted, and has sufficient space
Memory card data status
Shows the status of the content of the removable memory card.
The available values are:
  • Mismatch
    . Content of the removable memory card does not match the running configuration and/or firmware
  • OK
    . Running configuration and firmware matches the data on the memory card
Connections
Shows the number of CIP connections currently open to and through the adapter.
The available values range from 0 to 32767.
Packets lost
Shows the running sum of the number of Sequenced Address Item Sequence Numbers that are skipped in Class 0 and Class 1 connections consumed by the adapter and its children.
The available values range from 0 to 2147483647.
Timeouts
Shows the running count of the number of connections that time out, both originated and targeted, to and through the adapter.
The available values range from 0 to 2147483647.
HMI packet rate
Shows the rate at which the HMI packets are being sent and received.
The number of Class 3 packets and unconnected packets sent and received by the device in the previous second.
The available values range from 0 to 2147483647.
IO packet rate
Shows the rate at which the I/O data is being sent and received.
The number of Class 0 and Class 1 packets that were sent or received by the adapter in the previous second.
The available values range from 0 to 2147483647.
EtherNet errors
Shows the sum over all ports of the following EtherNet Link object values: In Discards, In Errors, In Unknown Protos, Out Discards, Out Errors, Alignment Errors, FCS Errors, Single Collisions, Multiple Collisions, SQE Test Errors, Deferred Transmissions, Late Collisions, Excessive Collisions, MAC Transmit Errors, Carrier Sense Errors, Frame Too Long, and MAC Receive Errors.
The available values range from 0 to 2147483647.
Flash update required
Shows whether the device requires application firmware.
The available values are:
  • True
    . Device has no application firmware. This can occur if the firmware update process is interrupted, or the device shipped without the application firmware.
  • False
    . Device has application firmware
Network status
Shows the current status of the network.
Supervisor status
Shows the current status of the supervisor.
Time Synchronization Status
Shows whether the device is currently synchronized with a Precision Time Protocol (PTP).
The available values are:
  • Synchronized
  • Not Synchronized
Grand master clock identity
Shows the identity of the Grand Master clock to which the device is synced.
The valid value is an 8‑byte hex number.
Local clock offset to system time
Shows the offset, in nanoseconds, from the local clock to the system time.
Use this value to detect steps in time. This value updates when a PTP update message is received.
The available values range from -9223372036854775808 to 9223372036854775807.
Local clock offset timestamp
Shows the timestamp of the local clock offset in YYYY-MM-DD-HH:mm:SS_mmm_uuu_nnn (UTC-00:00) format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
  • uuu = microseconds
  • nnn = nanoseconds
  • UTC-00:00 = Time zone
Possible values are a valid time or
None
if there is no recorded event time.
Over temperature
Shows whether the device is at a normal or higher temperature than its rated operating limits.
The available values are:
  • Yes
    . Device is at a higher temperature than its rated operating limits
  • No
    . Device is at a temperature within its rated operating limits
Over temperature timestamp
The time when an over temperature condition was most recently detected.
Possible values are a valid time or
None
if there is no recorded event time.
Critical temperature
Shows whether the temperature is above or below the critical temperature limit for proper operation.
The available values are:
  • Yes
    . Device is above critical temperature limit for proper operation and may shutdown without further warning
  • No
    . Device is not above critical temperature limit for proper operation
Critical temperature timestamp
The time when a critical temperature condition was most recently detected.
Possible values are a valid time or
None
if there is no recorded event time.
Low system power alarm
Shows whether the input system power voltage has moved below the configured Low System Power Limit.
If the input system power voltage is below the configured Low System Power Limit, the alarm remains set until the input system power voltage moves above the configured Low System Power Alarm Limit.
The available values are:
  • Yes
    . Power voltage is below configured Low System Power Limit
  • No
    . Power voltage is not below configured Low System Power Limit
Low system power timestamp
The time when a Low System Power condition most recently transitioned from No to Yes.
Possible values are a valid time or
None
if there is no recorded event time.
High system power alarm
Shows whether the input system power voltage moves above the configured High System Power Limit.
If it is above the configured High System Power Limit, it remains set until the input system power voltage moves below the configured High System Power Alarm Limit.
The available values are:
  • Yes
    . Power voltage is above configured High System Power Limit
  • No
    . Power voltage is not above configured High System Power Limit
High system power timestamp
The time when a High System Power condition most recently transitioned from No to Yes.
Possible values are a valid time or
None
if there is no recorded event time.
Internal fault
Shows whether an internal fault is present.
Internal fault timestamp
The time when an internal fault most recently occurred.
Possible values are a valid time or
None
if there is no recorded event time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal