Configure Dual-IP Mode in FactoryTalk Linx

You can configure the controller for Dual-IP mode with
FactoryTalk® Linx
software. You set the IP Address and Network Mask on the Internet Protocol tab.
TIP:
We recommend that you use a USB connection from the workstation to the controller when you set the IP address and Subnet Mask.
IMPORTANT: With
ControlLogix®
5590 controllers, the Ethernet ports on the controller itself are labeled 1 and 2. In programming and communication software, the ports are described as A1 and A2.
Use this procedure to set the IP address on port 1 and port 2.
  1. Confirm that the project is online.
  2. Confirm that the controller is in one of the following modes.
    • Program
    • Remote Program
    • Remote Run
    You cannot change the IP address or subnet mask if the controller is in Run mode.
  3. From the Port pull-down menu, choose an Ethernet port.
  4. Choose Manually configure IP settings.
  5. Assign IP Address and Network Mask values.
  6. Click Apply.
    This image shows how to manually set the IP address for a port in Dual-IP mode in FactoryTalk Linx.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal