Dialog: Update security policy model to ensure redundancy

Use the
Update security policy model to ensure redundancy
dialog to update the security policy model for Redundant Chassis Pairs.
Dialog example
Dialog elements description
Item
Name
Description
Add missing IP addresses to the model
table
Outlines IP addresses that you must add to the model to ensure that Redundant Chassis Pairs are correctly configured.
Update properties of existing IP addresses in the model
table
Compares existing devices properties with discovered devices properties that you must apply to ensure that Redundant Chassis Pairs are correctly configured.
TIP:
The automatic update may not be possible in all cases. See Redundancy statuses.
If needed, edit the model manually and then validate the model again.
Add missing IP addresses to the model
checkbox
Adds IP addresses listed in
Add IP addresses
to the security policy model to add Redundant Chassis Pairs.
Update properties of existing IP addresses in the model if possible
checkbox
Updates IP addresses listed in
Update properties of existing devices in the model if possible
to add Redundant Chassis Pairs.
IMPORTANT: Selecting this option may remove conduits.
Update
button
Updates the security policy model.
To use this option, you must select at least one of these checkboxes:
  • Add IP addresses to the model
  • Update IP addresses of existing devices and create Redundant Chassis Pairs
Export report
button
Exports the
update the security policy model to ensure redundancy
report to a file.
Cancel
button
Closes the dialog without making any changes to the security policy model.
TIP: Use this option if you want to edit the security policy model manually and then validate the model for redundancy again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal