Reset a node

Reset the configuration of a node device to factory defaults.
  1. Select the gateway device that contains the node device to reset.
    • Select
      Canvas
      and then select a device.
    • Select
      Zones
      and then select a zone and a device.
    • Select
      Devices
      and then select a device.
  2. In
    PROPERTIES
    , next to the node to reset, select .
  3. IMPORTANT: Resetting device configuration to factory defaults is irreversible.
    In
    Reset device configuration to factory defaults
    , select
    Reset configuration
    .
A message displays and informs about the successful reset operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal