Configuring a Motion Direct Command

Motion Direct Commands let you issue motion commands while you are online without having to write or execute an application program. The commands are useful when you are commissioning or debugging a motion application.
The content of the Motion Direct Command dialog box varies depending on the command.
To configure a Motion Direct Command
  1. Click the
    +
    sign in front of one of these command groups to expand the list of commands you can choose from.
    • Motion State
    • Motion Move
    • Motion Group
    • Motion Event
  2. Configure the operands for the selected command, as appropriate.
    Refer to the Instruction Set Reference help for more information on specific operands.
  3. Click
    Execute
    to verify the instruction operands.
  4. If you are issuing a Motion Direct Command to a CIP Safety drive, a dialog box opens on the screen if the drive is not in the correct state, or the drive is already permitting motor torque in Program Mode.
    If you want to perform the operation while the safety controller is in Program Mode, click
    Yes
    to bypass the Safe Torque Off safety function. Skip to step 5.
    Click
    No
    to cancel the command and close the dialog box.
  5. Click the
    Motion Group Shutdown
    button to force all axes in the motion group into the Shutdown state.
  6. Click
    Close
    to close the Motion Direct Command dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal