Function Block Properties Dialog Box - Storage & Weight Arrays Tab Overview (MAVE)

The Moving Average (MAVE) instruction calculates a time average value for the In signal.
Use the
Storage Array
tab to select the tag for the moving average buffer and weight array buffer for the selected MAVE function block..
The following table describes the parameters available on the
Storage Array
tab:
Parameter
Description
Storage Array
Select the tag for the moving average array. This array must be at least as large as the
NumberOfSamples
parameter.
Weight Array (optional)
Select the tag for the weighted average array. This array must be at least as large as the
NumberOfSamples
parameter. Element [0] is used for the newest sample; element [n] is used for the oldest sample.
New Tag
Click the
Storage Array
box or the
Weight Array
box to select the array, then click
New Tag
to create a new tag for the selected array.
Weight Array Values table
Displays the values in the weight array.
Status
Displays read-only status information for blocks containing status bits. If none of the status bits are set, an
OK
message appears in this field. Otherwise, a list of the status bits that are set appears here. This list is comprised of the parameter names associated with the status bits, and typically explain which parameters were configured with invalid values.
Execution Order Number
Displays the block's execution number if the routine is in a verified state. If the routine is not yet verified, a
Routine not verified
message displays. Note that this item is read-only.
Never display description in a routine
Select this check box if you do not want the description to display in the routine.
OK
Click this button to add the selected item in the instruction list to the routine and close the
Function Block Properties
dialog box.
Cancel
Click this button to cancel any edits you have made and close the
Function Block Properties
dialog box.
Apply
Click this button to accept your changes and continue editing in the
Function Block Properties
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal