Deploying projects

Compile projects to
FactoryTalk Optix Applications
and then deploy the applications to client devices.
You can manage the client devices to which you deploy
FactoryTalk Optix Applications
. See Manage client devices and Deploy a FactoryTalk Optix Application.
For client devices not accessible in the network, you can export
FactoryTalk Optix Applications
from
FactoryTalk Optix Studio
and then import them to client devices. See Export a FactoryTalk Optix Application and Import a FactoryTalk Optix Application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.