Develop an icon that changes color
Configure an image of a conveyor that changes chassis color based on the associated alarm state.
NOTE:
Download a sample project:
ChangeIconColorBasedOnAlarm.zipPrerequisites
- To develop the project
- Arrange the interface elements.
Select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback