CLI command: connect
Use the
connect
command to connect FactoryTalk Optix Studio
to a running FactoryTalk Optix Application exposing an OPC
UA server.Syntax
"C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" connect
endpoint
[--silent]Parameter | Importance | Description |
|---|---|---|
endpoint | Required | The IP address of the endpoint to connect to. |
--silent | Optional | Make the command output non-verbose in the command prompt. |
Example
"C:\Program Files\Rockwell Automation\FactoryTalk Optix\Studio
1.6.0.626\FTOptixStudio" connect 192.168.1.100
Provide Feedback