Runtime method types
Methods are executed at runtime when an event occurs.
Local runtime methods
Local methods are exposed by project objects, including:
- Alarms
- Loggers
- Databases
- Graphical objects
For example,
Video
objects expose the Play
method that starts the video playback.Global runtime methods
Global methods are exposed regardless of the selected node. Global methods are divided into these categories:
- Variable commands
- Core commands
- Alarm commands
- UI commands
- Recipe commands
For example, the
Acknowledge all
method acknowledges all alarms.Provide Feedback