Checkbox
Set and view a Boolean value using select/unselect
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Checked | Checked | Interrupter status. To enable another interface object when the value is True, create a dynamic link between this property and the Enabled property of the object to be enabled | |
Text trimming | Elide | Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set | |
Word wrap | WordWrap | Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set | |
Events
Modified value
- BrowseName
Event that is triggered when the user changes the value of the control
Provide Feedback