Non-exclusive deviation alarm

Monitors the deviation from a setpoint value of variables relating to physical quantities. Activates when the value of the monitored variable has a deviation equal to or greater than the set value. When several limits of interest are reached consecutively, the alarm signals all the limits reached.
BrowseName
NonExclusiveDeviationAlarmController
SuperType
Non-exclusive limit alarm(NonExclusiveLimitAlarmController)

Properties

Name
BrowseName
DataType
Description
Set point value
Setpoint
Ideal value for the monitored variable.
High-high limit
HighHighLimit
(Inherited from Limit alarm)
High limit
HighLimit
(Inherited from Limit alarm)
Low limit
LowLimit
(Inherited from Limit alarm)
Low-low limit
LowLowLimit
(Inherited from Limit alarm)
Enabled
Enabled
(Inherited from Alarm controller)
Active
Active
(Inherited from Alarm controller)
Auto acknowledge
AutoAcknowledge
(Inherited from Alarm controller)
Auto confirm
AutoConfirm
(Inherited from Alarm controller)
Input variable
InputValue
(Inherited from Alarm controller)
Message
Message
(Inherited from Alarm controller)
Severity
Severity
(Inherited from Alarm controller)
Last event
LastEvent
(Inherited from Alarm controller)

Events

NonExclusiveDeviationAlarmType
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.