Exclusive rate of change alarm
Monitors the rate of change of the value of a variable in a set time. Activates when the rate of change of the value of the monitored variable reaches one or more set limits. When several limits of interest are reached consecutively, the alarm signals only the last limit reached.
- BrowseName
- ExclusiveRateOfChangeAlarmController
- SuperType
- Exclusive limit alarm(ExclusiveLimitAlarmController)
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Polling time | PollingTime | Reference interval for monitoring the rate of change of the variable value. | |
Events
ExclusiveRateOfChangeAlarmType
- BrowseName
Provide Feedback