Data input style

Global properties for all project data entry controls.
BrowseName
DataInputStyle
SuperType
Control style(ControlStyle)

Properties

Name
BrowseName
DataType
Description
Background color
BackgroundColor
If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property.
Border color
BorderColor
Color of the polygon border.
Text color
TextColor
Color of the text to display.
Focus background color
FocusBackgroundColor
Focus border color
FocusBorderColor
Focus text color
FocusTextColor
Input placeholder color
PlaceHolderColor
Sets the input placeholder color when the user does not enter any text.
Select Color
SelectionColor
Sets the color selected.
Select text color
SelectionTextColor
Sets the text color selected.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Border width
BorderWidth
Thickness of the object border.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.