Image column

Data grid object column that contains data represented with images.
BrowseName
DataGridImageItemTemplate
SuperType
Data grid template element(DataGridItemTemplate)

Properties

Name
BrowseName
DataType
Description
Path
Path
Path.
Width
Width
Width of the window. It can assume values greater than or equal to zero. The Auto value sets the width equal to the width of the content (in this case, in the absence of content the object collapses).
Height
Height
Height of the window. It can assume values greater than or equal to zero. The Auto value sets the height equal to the height of the content (in this case, in the absence of content the object collapses).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.