Vertical alignment
Alignment of the object on the vertical axis.
- BrowseName
- VerticalAlignment
Values
Value | DisplayName | Description |
---|---|---|
0 | Top | The top side is positioned on the top side of the container, except for the top margin. |
1 | Bottom | The bottom side is positioned on the bottom side of the container, except for the bottom margin. |
2 | Center | The center of the object is positioned in the center of the container, except for the top and/or bottom margins. |
3 | Stretch | Object height equals container height, except for the top and/or bottom margins. |
Provide Feedback