Font weight
- BrowseName
- FontWeightEnum
Values
Value | DisplayName | Description |
---|---|---|
100 | Thin | Specify a font weight with a value of 100 in the OpenType specification. |
200 | Ultra light | Specify a font weight with a value of 200 in the OpenType specification. |
300 | Light | Specify a font weight with a value of 300 in the OpenType specification. |
400 | Normal | Specify a font weight with a value of 400 in the OpenType specification. |
500 | Medium | Specify a font weight with a value of 500 in the OpenType specification. |
600 | Semi bold | Specify a font weight with a value of 600 in the OpenType specification. |
700 | Bold | Specify a font weight with a value of 700 in the OpenType specification. |
800 | Ultra bold | Specify a font weight with a value of 800 in the OpenType specification. |
900 | Black | Specify a font weight with a value of 900 in the OpenType specification. |
950 | Ultra black | Specify a font weight with a value of 950 in the OpenType specification. |
Provide Feedback