InformationModel.MakeObjectType(browseName)
Creates an object type derived from BaseObject and returns a corresponding
IUAObjectType
C# object.static IUAObjectType MakeObjectType(QualifiedNamebrowseName);
Arguments
- browseName(QualifiedName)
- TheBrowseNameof the new object.
Returns
- IUAObjectType
- A C# object that corresponds to the project object created.
Example
The following example shows an API that creates a
Motor (type)
object and returns a corresponding C# object, which is assigned to the motor
variable. The Motor (type)
object is then added to the parent node of the NetLogic.
var motor = InformationModel.MakeObjectType("Motor"); Owner.Add(motor);
Provide Feedback