System Requirements

FactoryTalk® Edge Gateway™
works within the system requirements of all
Rockwell Automation®
software products.
Hardware Requirements
FactoryTalk Edge Gateway
requires hardware that meets or exceeds these specifications:
  • GB of memory
  • Dual-core processor
Rockwell Automation
recommends at least 32 GB of available drive space for
FactoryTalk Edge Gateway
.
FactoryTalk Edge Gateway distributed version is deployed to edge nodes managed via FactoryTalk Edge Manager. An example of edge node hardware is the ASEM 6300B edge computers. Hardware must meet requirements. For more information on the supported hardware, including third-party hardware support, please refer to the FactoryTalk Edge Manager documentation.
Software Requirements
FactoryTalk Edge Gateway distributed version is a containerized application delivered and managed via FactoryTalk Edge Manager, which adheres to the FactoryTalk Edge Manager software.
FactoryTalk Edge Gateway standalone version requires the following software on the host computer:
  • Operating system
    FactoryTalk Edge Gateway
    runs on the following
    Windows®
    operating systems:
    • Windows
      10 Professional or Enterprise edition (64-bit)
    • Windows
      11 Professional or Enterprise edition (64-bit)
    • Windows
      10 IoT Enterprise 2016
    • Windows Server
      2012 Standard
    • Windows Server
      2016 Standard
    • Windows Server®
      2012 R2 Standard
When you install FactoryTalk Edge Gateway standalone version 1.04.00, the following softwares will be installed if not already present:
  • Microsoft .NET Framework version 4.8
  • Microsoft ODBC Driver 18.0 for SQL Server x64 version 18.0.1.1
  • OPC .NET API version 2.01.10600
  • FactroryTalk Diagnostics version 6.31
  • Windows Firewall Configuration Utility version 1.00.16
  • CodeMeter Runtime Kit version 7.51.5429
  • Electronic Data Sheets Reader version 35.0.13
  • FactoryTalk Services Platform version 6.31.00
  • FactoryTalk Activation Manager version 5.00.12
  • EtherNet IP Address Commissioning Tool version 2.01.00
  • FactoryTalk Updater Agent version 4.00.00
  • Rockwell Automation x64 Driver version 2.03.06
FactoryTalk OPC UA functionality was tested with Kepserver EX.
Supported Browsers
The following web browsers have been tested and are supported for use with this release:
  • Google®
    Chrome™ browser
  • Internet Explorer®
    11
  • Mozilla®
    Firefox®
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal